Technical FAQs

Ask a Question

Are repair parts available for the ATS48 power terminals?

Issue:
Are repair parts available for the ATS48 power terminals?

Product Line:
ATS48 Altistart 48

Environment:
All

Cause:
Damaged terminal needs to be replaced.

Resolution:
None of the captive compression power terminals or the bus bar power terminals are offered as a repair part.  If damaged, the entire ATS48 will need to be replaced.
Was this helpful?
What can we do to improve the information ?