Technical FAQs

Ask a Question

What is the response time of the Run Permissive function of the ATV212 series drive?

Issue:
What is the response time of the Run Permissive function of the ATV212 series drive?

Product Line:
ATV212 series drives

Environment:
All models, All serial numbers

Cause:
Information unavailable in current literature.

Resolution:
The drive needs about 6 msec to manage the run permissive.
Details:
 => 2 ms for sampling on the terminal.
 => 2 ms for internal serial communication between microprocessors
 => 2 ms for treatments in the last subroutine.
So, from the time the Run Permissive is removed from the drive, it will take up to 6ms for the drive to respond accordingly.

 
Was this helpful?
What can we do to improve the information ?