Technical FAQs

Ask a Question

Powerpact B

Product Line:
Powerpact B

Resolution:
The PowerPact B circuit breaker is a new 125A MCCB introduced in late 2016, replacing the Legacy FAL/FHL and FA/FH circuit breakers. The Powerpact B is the smallest breaker in the Square D PowerPact range.
Here are just a few highlights:
-125A maximum rating
-small physical size
-high interrupting versions
-thermal/magnetic trip
-integrated DIN rail mounting
-field installable accessories
-flexible options for wiring terminations
-EverLink™ creep-compensating power wire terminals

For details, click the link to the product catalog 0611CT1603 (large file)
Was this helpful?
What can we do to improve the information ?