Technical FAQs

Ask a Question

What lugs come installed on MCP JJL36250M75?

Issue:
Need to know what lugs come installed on motor circuit protectors JJL36250M75 and JLL36250M75

Product Line:
Motor Circuit Protectors

Environment:
Electrical Distribution Equipment

Resolution:
Motor circuit protectors JJL36250M75 and JLL36250M75 come with lug kit AL175JD (#4 to 4/0AWG) installed on line and load ends. For the larger lug kit AL250JD (3/) to 350kcmil) on both ends, order MCPs with "LH" suffix.
Was this helpful?
What can we do to improve the information ?