Technical FAQs

Ask a Question

Can the circuit breaker operating handle in a J250AWK, J250DS and J250SS circuit breaker enclosures be operated without requiring the cover to be opened?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosures

Cause:
Clarification on product features

Resolution:
Yes, the NEMA Type 12, 12K and 4/4X/5 stainless steel circuit breaker enclosures have an external operating handle located on the right side wall. The enclosed circuit breaker is operated using the external operating handle.
Was this helpful?
What can we do to improve the information ?