Technical FAQs

Ask a Question

What is the replacement 200A fused switch assembly for a Model 6 MCC feeder bucket?

Issue:
What is the replacement 200A fused switch assembly for a Model 6 MCC feeder bucket?

Product Line:
Model 6 MCC

Environment:
Maintenance

Cause:
Replacement

Resolution:
NOTE Breakout parts drawing below :

 40555-127-50  200A FUSE BASE ASY   Qty 6 per fuse base. Item 20 on the dwg. 

The class R fuse clip is pn HRK1020  Qty 1 (this is a kit) Item 55 on the dwg.     

The mounting pan is pn 80409-010-01  item 25 in the dwg. 

The 200A fusible branch feeder uses a JLP36000S25 molded case switch. The handle mech asy is built into the left side of the saddle p/n 80420-349-52.
NOTE  The Branch Saddle dwg below,  Item #1 in the dwg:
 
Was this helpful?
What can we do to improve the information ?