Technical FAQs

Ask a Question

What color is the VW3A31817 conduit kit?

Issue:
Updated the FAQWhat color is the VW3A31817 conduit kit?
 
Product Line:
ATV212

Environment:
ATV212HD11M3X, ATV212HD15M3X, ATV212HD18M3X, ATV212HD15N4, ATV212HD18N4, ATV212HD22N4S
 
Cause:
2 colors shown in documentation

Resolution:
Gold colored conduit kit contained a yellow chomemate material that was not Rohs compliant approximately  2004/2005. We changed to the current color silver color as a result.
Was this helpful?
What can we do to improve the information ?