Technical FAQs

Ask a Question

Is S383 an option with the Altivar 71 drives rated for 500/600 Vac?

Issue:
Is S383 an option with the Altivar 71 drives rated for 500/600 Vac?

Product Line:
Altivar 71 drives

Environment:
ATV71 ....Y
 
Cause:
Product Selection

Resolution
No, the S383 is not an option with the ATV71 ....Y versions.
Was this helpful?
What can we do to improve the information ?