Technical FAQs

Ask a Question

What is the part number of remote mounting kit for the ATV Process Drive keypad?

Issue:
What is the part number of remote mounting kit for the ATV Process Drive keypad?

Product line:
ATV Process, Altivar 630, ATV630

Environment:
All

Cause:
Customer wants to remote mount the ATV630 keypad.

Resolution:
The mounting kit part number is VW3A1112.  The keypad plugs onto the face of the kit. The installation maintains an IP65 degree of protection.
A cable is required to connect the keypad in the mounting kit to the drive.

Cable length options:
VW3A1104R10 - 1 meter
VW3A1104R30 - 3 meter
VW3A1104R50 - 5 meter
VW3A1104R100 - 10 meter
Was this helpful?
What can we do to improve the information ?