Technical FAQs

Ask a Question

Is it possible to add multiple bluetooth dongle to multiple drives then connect to each drive directly through Somove?

Issue:
Is it possible to add multiple bluetooth dongle to multiple drives then connect to each drive directly through Somove?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
They want to add a bluetooth dongle to each drive like 10 of them then connect to each drive via somove. 

Resolution:
The bluetooth dongle is not designed for this use.  Its recommended that you use one dongle and connect that dongle to the drive that you would like to commission with somove.  Example: If you have 10 drives you would take the one bluetooth dongle connect to one drive then connect to somove.  Once you are done remove the dongle from that drive and then connect it to the second drive. 
Was this helpful?
What can we do to improve the information ?