Technical FAQs

Ask a Question

What is the speed range on the ATV71 drives?

Issue:
What is the speed range on the ATV71 drives?

Product Line:
ATV71

Environment:
 All

Cause:
Additional Documentation Request

Resolution:
Speed range
1…599 in closed loop mode with encoder feedback
1…100 in open loop mode
Was this helpful?
What can we do to improve the information ?