Technical FAQs

Ask a Question

Is it possible to have five light units and an audible on an XVB

Issue:
Is it possible to have five light units and an audible on an XVB

Product Line:
XVB

Environment:
Stack/Tower Lights

Resolution:
No. It only has 5 terminals and therefore can only control a max of 5 outputs
 
Was this helpful?
What can we do to improve the information ?