Technical FAQs

Ask a Question

ATV58 with the optional VW3A58310U ethernet card how can you change the timeout setting on the web page?

Issue:
ATV58 with the optional ethernet card how do you change the timeout setting on the web page?

Product Line:
Altivar ATV58 with the optional VW3A58310U option card. 

Environment:
All

Cause:
Wants to change the timeout setting on the web page 

Resolution:
The following operations are required to modify the Time Out value:

1. Enter No in the I/O Scanner field.

There may be a delay before the page updates, depending on the

capacity of your computer.

2. Modify the Time Out value. Now hit the enter and then save.

3. Enter Yes in the IoScanner field.

4. Click the Save button to confirm your modifications, or click the abort button to cancel
 
Was this helpful?
What can we do to improve the information ?