Technical FAQs

Ask a Question

What do the 3 LEDs flashing mean on the ATV312?

Issue: 
What do the 3 LEDs flashing mean on the ATV312?
 
Product Line:
Altivar 312
 
Environment:
All serial numbers
 
Cause:
N/A
 
Resolution:
When the ATV312 is in local mode by pressing and holding the “MODE” button for 3 seconds, the three LEDs (REF, MON and CONF) are strolling.   In order to make parameter changes while in local mode, you have to press and hold the esc key for 2 seconds, the three LEDs (REF, MON and CONF) flash together, meaning the drive is in programming MODE,  while in local mode.  
 
Was this helpful?
What can we do to improve the information ?