Technical FAQs

Ask a Question

Confirmation Email from Conext Insight Not Being Received

Issue:
Unable to log into Conext Insight, and have not received confirmation email.

Environment:
Conext Insight Registration

Resolution:
Verify that the user is logging in to http://conextinsight.schneider-electric.com
There is a demo version of Conext Insight available on sesolar.com that is not for actual use.  A sign that the user is on that site is the graphic in the top left showing "Demo Conext Insight".  If they try to log in to the demo version with an account created in the demo version, the user will also get a script error.

Demo address is: http://conextinsightdemo.cloudapp.net/en

Cause:
Trying to register for a new Conext Insight account using the demo version of the website.
 
Was this helpful?
What can we do to improve the information ?