Technical FAQs

Ask a Question

What communication options are available for the ATV21 and or SFD21 enclosed drives?

Issue:
What communication options are available for the ATV21 and or SFD21 enclosed drives?

Product Line:
Only ATV21 and SFD21 drives. 

Environment:
All

Cause:
Wants to add a network communication to an existing ATV21 and or SFD212 drives. 

Resolution:
Modbus is integrated and is standard.

The options were 
Lonworks:  VW3A21312
Metasys N2: VW3A21313
Apogee FLN P1: VW3A21314
BACnet: VW3A21315
Please note all of the options are no longer available and is obsolete and these cards will not work on the new ATV212 and SFD212 drives. 



 
Was this helpful?
What can we do to improve the information ?