Technical FAQs

Ask a Question

Can the ATS22 and ATS48 soft starters run with 50hz input power supply?

Issue:
Can the ATS22 and ATS48 soft starters run with 50hz input power supply?

Product Line:
ATS22 and ATS48 series

Environment:
All serial numbers for ATS22 and ATS48 series

Cause:
N/A

Resolution:
Yes, the soft starters can work with both 50/60 hz line power
Was this helpful?
What can we do to improve the information ?