Technical FAQs

Ask a Question

Converting NEMA 12 enclosure to NEMA 3R

Issue:
For the NEMA 12/3R enclosure option offered for the class 8502/8536 contactors and starters, it states as follows:

"Watertight conduit hubs or equivalent provision for watertight connection at the conduit entrance, when the conduit enters at a level higher than the lowest live part shall be used.
Drain holes of 1/8 inch diameter shall be added to the bottom of the enclosure."

Will this modification void the UL listing?

Product Line:
NEMA starters and contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications and Certifications

Resolution:
This modification will not void the UL listing of the device.
Was this helpful?
What can we do to improve the information ?