Technical FAQs

Ask a Question

Painted Stainless Steel Enclosures

Issue:
Is there an option for painting the stainless steel enclosures offered for class 8502/8536/8538 contactors and starters?

Product Line:
NEMA contactors and starters - GIC Product

Environment:
US Product

Cause:
Product characteristics and options

Resolution:
No, these enclosures cannot be painted at the factory as the paint will not adhere properly to these enclosures.
Was this helpful?
What can we do to improve the information ?