Technical FAQs

Ask a Question

Mounting RE17 Relays at a forward tilt

Issue:
Can the RE17 relays be mounted at a 45 degree forward incline?

Product Line:
IEC Control Relays - GIC Product

Environment:
US Product

Cause:
Product installation and characteristics

Resolution:
Yes, these relays can be mounted up to 45 degrees forward from vertical.
Was this helpful?
What can we do to improve the information ?