Technical FAQs

Ask a Question

XW Output Derating Based on Ambient Temperature.

Issue:
XW+ Ambient Temperature operating range and derating

Environment:
XW+ 6848 and XW+ 5548 in possible environments where ambient temperature can reach extremes.

Resolution:
Rated Temperature Range (meets specifications) 32-77 °F (0-25 °C)
Operational Temperature Range -13-158 °F (-25-70 °C)
Storage Temperature Range -40-185 °F (-40-85 °C)
see attachment for graphs


 
Was this helpful?
What can we do to improve the information ?