Technical FAQs

Ask a Question

What is the largest HP of ATV61 Plus drives?

Issue:
What is the largest HP of ATV61 Plus drives?

Product Line:
Altivar 61

Environment:
All
 
Cause:
Product Selection & Services

Resolution:
Altivar61  Largest size available
125 HP - 900 HP 460Vac
125 HP - 800 HP 575Vac
Was this helpful?
What can we do to improve the information ?