Technical FAQs

Ask a Question

ATV61 or ATV71: What is AI1 assignment?

ATV61 or ATV71: What is AI1 assignment?
Issue: 
ATV61 or ATV71: What is AI1 assignment?
 
Product Line:
Altivar 61, Altivar 71
 
Environment:
All serial numbers
 
Cause:
N/A
 
Resolution:
[AI1 assignment]
Read-only parameter, cannot be configured.
It displays all the functions associated with input AI1 in order to check, for example, for compatibility
problems.
Was this helpful?
What can we do to improve the information ?