Technical FAQs

Ask a Question

RM5TF30 with backfeed

Issue:
Will the phase loss relay, RM5TF30 change state on phase loss if there is a substantial backfeed?

Product Line:
Measurement Relays - GIC Product

Environment:
US Product

Cause:
Product Operation and Characteristics

Resolution:
If a phase loss occurs and there is substantial backfeed to the relay, it is possible that the relay could be fooled into thinking that all three phases are present on a circuit.  Under typical applications, the "missing leg" would be of a voltage that is significantly different from the other present legs.  With tight enough thresholds, the relay can be set to change contact state just from the imbalance itself.
Was this helpful?
What can we do to improve the information ?