Technical FAQs

Ask a Question

Using TeSys U with Grounded Neutral

Can the TeSys U motor starters be used on a single phase system with a grounded neutral?

Product Line:
TeSys U - GIC Product
LUB12, LUB32

US Product

Product Application

Yes, these starters can be used in this type of setup.  If the power wiring is grounded at the motor as well, an imbalance between hot and neutral can result which can cause nuisance tripping.
Was this helpful?
What can we do to improve the information ?