Technical FAQs

Ask a Question

Which ATV71 drives do not contain Dynamic braking transistors?

Issue:
Which ATV71 drives do not contain Dynamic braking transistors?

Product Line:
ATV71 

Environment:
ATV71HC20N4, ATV71HC25N4. ATV71HC28N4, ATV71HC31N4, ATV71HC40N4, ATV71HC50N4, ATV71HC20Y, ATV71HC25Y, ATV71HC31Y, ATV71HC40Y, ATV71HC50Y, ATV71HC63Y   

Cause:
N/A

Resolution:
These products do not contain a dynamic braking transistor. A separate transistor must be added for applications requiring dynamic braking.
Was this helpful?
What can we do to improve the information ?