Technical FAQs

Ask a Question

Can an HDL26150 be used with an NQSFB2HJ ?

Issue:
Sub-feed breaker in NQ panel

Product Line:
Panelboards

Environment:
NQ

Cause:
2 pole breaker with 3p kit

Resolution:

 
 
No. The back pan and deadfront are setup for using a 3p breaker whether 2 or 3 poles are connected 
Was this helpful?
What can we do to improve the information ?