Technical FAQs

Ask a Question

Using the RM17TE00 on a High-leg Delta System

Issue:
Will the RM17TE00 phase loss relay work on a high-leg delta system?

Product Line:
Phase loss relays - GIC Product

Environment:
US Product

Cause:
Product Application

Resolution:
Yes, this relay can be used on this system.  The recommended configuration is to put the high-leg on L3 as shown in the attached document.
Was this helpful?
What can we do to improve the information ?