Technical FAQs

Ask a Question

Why is my Conext CL inverter stuck on the Initializing Screen?

1) The inverter is doing internal processing and may stay at the 'initializing' screen for up to 5 minutes after a firmware update. Note the current time and wait for five minutes

2) If system stays in 'initalizing' for over five minutes. 
     - Download the latest firmware for the inverter from the SESOLAR.COM website. Unzip the firmware to a good-quality USB thumb drive.  
     - Remove DC and AC power from inverter and insert thumb drive
     - Apply DC or AC power to inverter, wait for inverter to boot, and accept prompt to upgrade firmware
     - Upgrade firmware as per  owner's manual 

Contact your local Schneider Electric customer care team if problem persists
Was this helpful?
What can we do to improve the information ?