Technical FAQs

Ask a Question

Are the M-Flex drives CE Cerified?

Issue:
Are the M-Flex drives CE Cerified?

Product Line;
ATV61/ATV71

Environment:
All M-Flex enclosures

Cause:
Are the M-Flex drives CE Cerified?

Resolution:
The M-Flex enclosures do not have the CE certification.
There is a option for CSA, but not CE.
 
Was this helpful?
What can we do to improve the information ?