Technical FAQs

Ask a Question

What is the 1209 suffix?

Issue:
What is the 1209 suffix?

Product Line:
Molded Case Circuit Breakers

Environment:
Legacy Breaker Suffixes

Cause:
What is the 1209 suffix?

Resolution:

The 1209 suffix indicates a 3A3B aux contacts with gold flash contacts, a normally open bell alarm switch, a 48 Vdc undervoltage trip, and special 48 inch leads for the accessories.


Keywords: 1209 suffix suffixes accessory accessories normally open bell alarm switch switches gold flash contact contacts aux auxiliary 48 Vdc V dc uvr undervoltage release relay trip left right pole 48 in inch lead leads
Was this helpful?
What can we do to improve the information ?