Technical FAQs

Ask a Question

Can TVS4EMA Surge Protective Devices (SPD) be used for 480/240V 3 phase/ 4 wire B high leg Voltage systems?

Issue:
Can TVS4EMA Surge Protective Devices (SPD) be used for 480/240V 3 phase/ 4 wire  B high leg Voltage systems?

Product Line:
TVSS SPD

Environment:
Application

Cause:
Clarification

Resolution:
No, only 480/Y277V usage is recommended  . SQ D /Schneider Electric does not have a product offering for a 480/240V B High Leg voltage systems
Was this helpful?
What can we do to improve the information ?