Technical FAQs

Ask a Question

Can the Motor Run Time (rtH) on the Altivar Process drives be adjusted between seconds, minutes or hours?

Issue:
Can the Motor Run Time (rtH) on the Altivar Process drives be adjusted between seconds, minutes or hours?

Product Line:
Altivar Process

Environment:
All serial numbers for Altivar Process

Cause:
N/A

Resolution:
No the run elasped time display is resettable in either seconds, minutes, or hours. This all depends on the length of time the motor has been running.
Was this helpful?
What can we do to improve the information ?