Technical FAQs

Ask a Question

Can the Motor Run Time (rtH) on the Altivar Process drives be adjusted between seconds, minutes or hours?

Issue:
Can the Motor Run Time (rtH) on the Altivar Process drives be adjusted between seconds, minutes or hours?

Product Line:
Altivar Process

Environment:
All serial numbers for Altivar Process

Cause:
N/A

Resolution:
No the run elapsed time display is not resettable in seconds, minutes, or hours but it is not adjustable
Was this helpful?
What can we do to improve the information ?