Technical FAQs

Ask a Question

Where can I find programming assistance on setting up the ATV312 drive with the optional VW3A31209 Devicenet option card?

Issue:
Where can I find programming assistance on setting up the ATV312 drive with the optional VW3A31209 Devicenet option card?

Product Line:
Altivar ATV312

Environment:
All with the VW3A31209 Devicenet option card

Cause:
Needs to set up the ATV312 drive with the ethernet option card. 

Resolution:
For ATV312 Devicenet programming assistance please reference the S1A10387 installation manual. 

 
Was this helpful?
What can we do to improve the information ?