Technical FAQs

Ask a Question

How do I show the motor run time (RTH) in hours instead of seconds?

Issue:
The Altivar Process Drive Programming Manual dated 05/2014 states "Motor run time.Run elapsed time display (resettable) in seconds, minutes, or hours (length of time the
motor has been switched on)."


Product Line:
ATV630 Process Drive

Environment:
All models and serial numbers.

Cause:
Documentation error

Resolution:
The description in the programming manual dated 05/2014 is incorrect. In terms of RTH, its unit is 1s at present.  According to function diagram, monitoring parameter are display in unit defined by Cfg_Unit.  However, Cfg_Unit isn't used for ATV630 platform. So the unit of RTH and PTH can not be configured. It only can display in seconds. And we will inform the document department and update the manual.
 
Was this helpful?
What can we do to improve the information ?