Technical FAQs

Ask a Question

What changes are made to an S-Flex that is ordered with serial communications options A06 B06 C06 D06?

Issue:
What changes are made to an S-Flex that is ordered with serial communications options A06 B06 C06 D06?

Product Line:
S-Flex 212

Environment:
All

Cause:
Standard card has most options already imbedded

Resolution:
Serial communications for BACnet(A06), Metasys N2(C06) and Apogee FLN P1(D06) are imbedded in the standard control card.  Ordering the option on an S-Flex will change factory settings:
Network protocol F829 = 2 for Metasys, 3 for Apogee, 4 for BACnet
Command mode CMOd = 2 for serial comms control of Start/Stop
Frequency mode FMOd = 4 for serial comms control of Speed Reference

The LonWorks(B06) option replaces the standard card with a LonWorks card (VW3A21212), sets F829 = 5, CMOd = 2 and FMOd = 4.
Was this helpful?
What can we do to improve the information ?