Technical FAQs

Ask a Question

Can the ATV18 drive be programmed for an internal PID feedback setup?

Issue:
Did the Altivar ATV18 drive have an internal PID feedback option?

Product Line:
Altivar ATV18

Environment:
All

Cause:
Wanted to know if the ATV18 drive had an internal PID setting option.

Resolution:
Yes the ATV18 drive did have a internal PID feedback assignment.

AIC Assignment of the analog input AIC/AI2.
If the logic inputs are not assigned to
PS2, PS4 or JOG, the choices are:
SAI SAI PIF Config.
SAI: Reference summing with AI1
PIF: PI feedback. This configuration automatically assigns AI1 as PI set point input and causes rPG,
rIG, and FbS to appear in the Level 1 parameters.
Note: PIF is only possible if the logic inputs have previously been assigned as follows in this order:
1) LI4 = OFF or FSt
2) LI3 = OFF or dCI
3) LI2 = OFF or rrS 


 
Was this helpful?
What can we do to improve the information ?