Technical FAQs

Ask a Question

Is the ATV12 drive available in 460V?

Issue:
Customer wants the ATV12 drive for a 5HP, 460V motor.

Product line:
ATV12, Altivar 12

Environment:
all

Cause:
n/a

Resolution:
The ATV12 model is only available for 208-230V motors.  For 460V ratings, use the ATV312 drive which has units available up to 20HP, 460V.
Was this helpful?
What can we do to improve the information ?