Technical FAQs

Ask a Question

What is the V09 mod on the E-Flex enclosed drives?

Issue: 
What is the V09 mod on the E-Flex enclosed drives?

Product Line:
8839 E-Flex

Environment:
All

Cause:
Needs the Ethernet IP card option.

Resolution:
Mod V09 is the Ethernet VW3A3316 option card installed in the E-Flex enclosed Drive. 
Was this helpful?
What can we do to improve the information ?