Technical FAQs

Ask a Question

Can the ATS01N125FT soft starter be used on single input voltage and run a single phase motor?

Issue:
Can the ATS01N125FT soft starter be used on single input voltage and run a single phase motor?

Product Line:
ATS01

Environment:
Only ATS01N125FT

Cause:
Wants to run a 1 phase motor with 1 phase input power on this ATS01N125FT

Resolution:
According to product engineering this ATS01N125FT is only rated for 3 phase voltages and 3 phase motors.  It is not rated for 1 phase voltage and 1 phase motors. 
Was this helpful?
What can we do to improve the information ?