Technical FAQs

Ask a Question

Does the ATV61 have 6 pulse front end?

Issue: 
Does the ATV61 have 6 pulse front end? 

Product Line:
ATV61, ATV71 

Environment:
Standard 

Cause:
NA

Resolution: 
Yes, the ATV61/71 have a 6 pules front end. 
Was this helpful?
What can we do to improve the information ?