Technical FAQs

Ask a Question

Can I power up the ATV66 power board with the control board removed?

Issue: 
Can i power up the power board with the control board removed? 

Product Line: 
ATV66

Environment:
ATV66

Cause:
Testing 

Resolution: 
Understand that powering on the Power board with Control board   removed will not damage the Power board ; however, Schneider is recommending, probably for safety reasons, not to power on the Power board  with Control
 board removed.
Was this helpful?
What can we do to improve the information ?