Technical FAQs

Ask a Question

ATV630 - are there terminating resistors for Modbus built into the drive?


Issue:
ATV630 - are there terminating resistors for Modbus in the drive?

Product Line:
ATV630

Environment:
Modbus

Cause:
Terminating Resistors for Modbus

Resolution: 
No, ATV6xx/9xx does not have embeded terminating resistors for Modbus. 
If needed, they have to be implemented external to the drive. 


 
Was this helpful?
What can we do to improve the information ?