Technical FAQs

Ask a Question

What is the factory default password for the VSD57?

Issue:
What is the factory default password for the VSD57?

Product Line:
Variable speed drives

Environment:
VSD57

Cause:
Customer wants to know what is the default password to access the menus for programming the drive.

Resolution:
Factory default password Level 1 is 9100
Factory default password Level 2 is 0019

Keywords:
VSD57, default password
Was this helpful?
What can we do to improve the information ?