Technical FAQs

Ask a Question

Is there an English language version of the ATV303 (Altivar 303) manual available?

Issue:
Customer is looking for an English manual for a drive (ATV303) that is only built and sold in China.

Product Line:
ATV303, Altivar 303

Environment:
All part numbers

Cause:
Product is specifically built for the Chinese market.  It is not sold or supported in the US, however some customers have received the drive on Chinese built equipment.

Resolution:
The ATV303 drive is one that has only been released for sale in China. 
It is not sold or supported in the US.
An English version of the manual is provided here as a resource to any customers who may need it, but support for this product must come from the vendor who supplied it.

We make no guarantees that this manual is the most recent version.   It is provided as a courtesy.  Customers should check with the OEM who provided the drive to determine if a more recent version is available.
Was this helpful?
What can we do to improve the information ?