Technical FAQs

Ask a Question

ATV312 What would stop the drive from running in terminal mode with a remote HMI connected?

Issue: 
ATV312: What would stop the drive from running in terminal mode with a remote HMI connected?

Product Line:
ALTIVAR 312

Environment:
All
 
Cause:
Installation / Setup

Resolution:
Verify LCC is not set to "Yes". 
Verify programming is set for terminal control, not local controls.
Was this helpful?
What can we do to improve the information ?