Technical FAQs

Ask a Question

What is the master password in order to unlock the Altivar 31/312 Drive, if the password is forgotten.

Issue:
What is the master password in order to unlock the Altivar 31/312 Drive, if the password is forgotten.

Product Line:
All ATV31/312 drives 

Environment:
All ATV31/312 drives

Cause:Password for ATV31/312 drives

Resolution:
The master password in order to unlock the Altivar 31 Drive is 6969.

This code overrides and resets the set password

Was this helpful?
What can we do to improve the information ?