Technical FAQs

Ask a Question

I cannot select option B08 for my E-Flex drive

Issue:
E-Flex, ATV61Customer requested option B08 for his E-flex but the selector does not allow it. 

Product line:
E-Flex without bypass. 

Environment:
all

Cause:
Customer was ordering 8839EFD***VWxxxx.  The W in the part number indicates no bypass option. 

Resolution:
Modification B08 includes a pilot light for the bypass mode.  Since there is no bypass in this drive, they cannot select that.  Use Mod C08 which comes with the same pilots as B08 except no bypass pilot.  (Red 'on', Green 'run', Yellow 'fault')
Was this helpful?
What can we do to improve the information ?