Technical FAQs

Ask a Question

Can the ATV66 communicate by way of Ethernet?

Issue:
ATV66 Ethernet

Product Line:
ATV66

Environment:
All models and serial numbers

Cause:
None

Resolution:
No Ethernet available.  However, some third party modbus to ethernet gateway devices can be used.  See the attached for a list.  The communication protocols available on the ATV66 are Uni-Telway, Modbus RTU/Jbus, Modbus ASCII network.  
Was this helpful?
What can we do to improve the information ?